The Universal Driver support multiple version of 32 and 64 bit windows in a single installation package. The installed driver will support current e-BRIDGE products and most of the older e-BRIDGE products. This driver supports Windows 2000 through Vista.
Use this driver primarily in installations with multiple different MFPs so as to present the user with a single user interface for the multiple products. Since these driver as based in the Windows mini-driver development package, there may be additional circumstances where these drivers present a more appropriate choice in considereation of the users full computing environment.
This driver does not support products with the Fiery controller installed.